I’ve got a few questions regarding the DLP Lightrafter Evaluation Module. I've looked a bit through this forum, but there are a lot of questions and appereantly a lot of people helping, so i thought of giving this a try.
I’m looking for a simple module including a DMD Chip and a Controll unit for this DMD chip. There are versions like the W4100, but they are a bit expensive. Currently i’m thinking of using this above named Evaluation Kit.
Is it possible to disable the light engine/LEDs without deactivating the DMD?
Can you also remove the Light engine/LEDs and the lense, so that you’ve just got the DMD and the control device? Or are there any problems, e.g. with the heat sink?
Is there an extra variation for this 0.3WVGA DMD, maybe even for UV like for the DLP7000/DLP700UV? Or are these specifications only depending on the window?
And a few minor questions, because i'm just a little bit confused :
Are there any known compatibility problems regarding Windows 8 or 10?
There is one Micro-SD slot. Is a Micro-SD really necessary for using the DMD? If yes, will there be one included in this Kit?
And the last one for the 0.3WVGA: This Chip is using what is commonly known as „diamond“ pixels, am i right?
Thanks in advance for your help, and really sorry for my english, if you were confused.
Till