Hi,
I have 2 DLP® LightCrafter™ Evaluation Modules with the LEDs removed. The two of them have stopped working due to MSP430 protection modes as I can see in led D3:
- System voltage less than 3.8 V or greater than 5.2 V
- Light engine thermistor above 70°C
I would like to skip these shutdown protection modes. How can I do it?
Thanks, Pepe