Hello,
we are using DLP LightCrafter EVM with DLP3000 in a scientific application for the purpose of optics calibration. Our partial interest is the micromirror's lateral position accuracy - whether it is specified or not, some "worst case" estimations etc.?
The only reference for the accuracy we can find in datasheets is the size of active array, especially amount of digits after a decimal point (we can see 4 digits, so the estimate would be 100nm), but this is not stated clearly, as well as other geometrical characheristics (adjacent mirrors accuracy, field distortion, dimension calibration accuracy).
-------
Thanks for any information,
Fedor Inochkin