Hi,
As I said, after having troubles with my last TWO Lightcrafter I bought YET ANOTHER one.
Opened the LCr, powered it on, connected to my PC, and what I see is the following:
- The splash/pattern screen does not show. Instead, it flashes for a small fraction of second every 30 seconds or so
- If I see my Network connection it appears as the LCr connects as RNDIS device but immediately it disapears. It is connecting and disconnecting
- The LED's are not showing any shutdown protection mode.
- The LCr has not been modified at all.
- I see the current consumption is 380 mA up to 400 mA sometimes
- I see the voltage on my power supply is 5.20 V
I found this insane, I mean this is the third one LCr I bought and three were problematic ones???!!
Please help!