I have been trying to display the HDMI input with no luck. I have a LightCrafter 4500 connected to my laptop. Since I cant direct connect the HDMI connector I have an adapter to Display port. I am running LightCrafter GUI Version 1.2. Both the laptop and GUI detect the LightCrafter 4500. I am able to configure the laptop to to use the projector but nothing is ever displayed on the projector. I believe its something Im doing or not. Im able to change the images that are stored locally on the LC. Able to set the LED's. But still not 100% sure on how to set the LC to use and project the image from the HDMI input. Is there any detailed step by step on how to configure the HDMI input? Or does LC able to autodetect?