I am interested in knowing if it is possible to user swap the 0.45 DLP chip in the Lightcrafter with the 0.45 DLP NI chip?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am interested in knowing if it is possible to user swap the 0.45 DLP chip in the Lightcrafter with the 0.45 DLP NI chip?
Hello Ernesto,
Yes, you can swap with 0.45 DLP NIR chip. Only comment we have is you should be aware about the standard light engine that comes with the Kit, and the optical elements are optimized for the Visible light Spectrum, you may not get the maximum efficiency because first, DMD is optimized of NIR (Near-IR) range secondly, the input source in the light engine R G B LEDs fall under visible light spectrum.
Regards,
Sanjeev