Hi,
We are interested in buying a LighterCrafter 4500. I would like to ask a few questions about this module.
(1) From an earlier post, it seems that the DMD is attached in the iView light engine and connected to the board using a flexible cable. And it seems possible to separate the DMD from the rest of the light engine. So, after the separation, how can I mount the DMD? Can I directly attach the DMD back to the LIghtCrafter with screws? If not, do I need to make my own part to mount the DMD?
(2) We would like to use an external trigger to control the DMD. We want to store some 1-bit patterns into the DMD memory. Is LightCrafter 4500 capable of doing this? And how fast can the DMD operates under this mode?
(3) How reliable is this device? We had some difficulties using the LightCrafter 3000. Although claimed to work well, the external triggering never worked for our device, which forced us to go with the video streaming mode. Have you really fixed all previous problems in LightCrafter 3000?
Thank you,
Jinyang