Dear all,
I have a question about the synchronization between camera and projector.
I use labview to come up changing patterns as pattern source. The changing patterns come through HDMI into the projector.DLP4500 is set to pattern mode via video port. The Vsync period is 16667 us and the pattern exposure is 9000 us.I only use G0 as pattern sequence and "Trigger 2 pattern per pulse " is set to 12. So ,the camera triggered by trigger out 2 is triggered once every 200ms.
Return to labview, I make the pattern change once every 200ms .
Theoretically,the camera and the projector can be synchronized.When the pattern changes,the camera takes one photo.However, the result is not so and has some laws.In most cases,it works normal in first 3 photos but the forth one is the same as the previous one. Then it repeats in this cycle.
How can i make them totally synchronized?
In other posts ,I find they use API to project. I wonder if i can project video via API(and how).
Thank you in advance for your attention
Jiong