I also have same question on how to make LightCrafter 4500 running flash pattern automatically after boot.
Situation:
I successfully made a pattern sequence by LCR4500GUI, running well by press "play" on tab "pattern sequence" -"sequence setting" page.
I try to make the sequence automatic running after power on boot.
So, I press "save solution", set .ini file as attached file, and upgrade the PROM firmware.
DEFAULT.AUTOSTART 0x0 ;
DEFAULT.DISPMODE 0x1 ;
The user manual described "0x1 = Pattern display mode (will start pattern sequence after initialization and splash time-out)
I suppose the pattern sequence will running automatically, but it didn't.
Questions:
1. where to find the solution on user guide? the mentioned section 2.11 did not existed on user guide (doc#DLPU011D)
2. user manual described DEFAULT.PATTERNCONFIG.TRIG_MODE 0x01:Internal or external trigger
How to make sure the internal trigger is enable, instead of waiting an external trigger ?
Best Regards,
Simon