Hello,
we have problems with our own DLPC350 board. Our board is based on the Lightcrafter reference design.
The problem is, that we can't program the M29W128 flash memory on our board. We are using the UM232H and the JTAG flash programming utility fromTI.
If we scan the JTAG chain the DLPC350 is detected. Then we start the programming of the flash. This takes about 20min to complete to 100% (yes, we were very patient...)
After this we power-cycle the board, but the init_done is always low. We then tried to readback the flash. The content of the flash is empty.
It seems to me that the flash_parameters.txt is not correct for only one M29W128. The lightcrafter design has two M29W128. Is it possible to use this tool, with only one flash ?
What about the boardfile ? Do we have to edit it ? And if so, which parameters should be filled in ?
Any further suggetion?
greetings
Lars