When I plug it into an ATI Firepro v9800, it comes up as a Generic PnP Monitor in windows 7 that has a resolution of 640x480 63 hertz (there are no other options to choose from). Is there someway to get it to 480x320? Is there some driver I need to download or some procedure I need to follow?
Thanks!
Chris,
The Pico Kit v2 always requires 640x480@60Hz - not 480x320 (which is the native resolution of the DLP1700 DMD). The internal EDID reports the Pico Kit v2 resolution as 640x480. So, the resolution which your OS is showing is probably the correct one. (For now I wouldn't worry about the 63Hz.) When you duplicate or share the Win7 screen does it show on the Pico Kit?
Best regards,
Pascal