Hi,
I have a trouble to make an application software with D4100 ActiveX. I bought D4100 kit with 0.95" DMD and D4100 Explorer V1.(V1.0.0.0) and tried to use its ActiveX functions. When I used connectdevice() function, it returned "0". It was used right bin file, "D4100_GUI_FPGA.bin". It was tested windows XP and windows 7. The application software in the package worked in both windows system but my application didn't work.
I've used previous version, D4000 kit, D4000 software(ActiveX) and "usb_main.bin", there was no problem. I changed activex controller (DDC4000 -> DDC4100), function name and bin file. LabView and Labwindows/CVI were used.
DG