• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » DLP & MEMS » New DLP Applications & Technology Forum » All Tags » analog mirror
Share
DLP & MEMS
  • Forums

Browse by Tags

DLP & MEMS

Welcome to the DLP & MEMS Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Sign In to Post
Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
analog mirror
  • analog mirrors
  • Analog point mirror
  • MEMS
  • pointing mirror
  • TALP1000B
Related Posts
  • Forum Post: Welcome to the MEMS Analog Mirrors Forum!

    rmeza rmeza
    Welcome to the MEMS Analog Mirror forum! For over a decade TI has developed and manufactured MEMS-based analog mirrors for optical applications. Now TI is offering its analog mirrors on ti.com. Feel free to use this forum to discuss applications and questions for the analog mirrors with the TI E2E Community...
    on Sep 18, 2009
  • Forum Post: Analog mirror demos will be at SPIE Photonics West

    rmeza rmeza
    SPIE Photonics West will be January 26-28 in San Francisco. This year, you can check out demos using TI's analog mirror products (Booth #315) including a laser steering demo using the TALP1000B and a scanning mirror application for medical imaging. There will be several other demos featuring TI's...
    on Jan 4, 2010
  • Forum Post: TALP1000B samples available through TI eStore

    rmeza rmeza
    Based on feedback from its recent ti.com release, limited sample quantities of the TALP1000B dual-axis pointing mirror can now be purchased through the TI eStore. This eStore option allows purchase of 3 or 6 mirrors for evaluation. For quotes and availability of larger quantities of TALP1000B mirrors...
    on Dec 15, 2009
  • Forum Post: UV capable micro-mirror

    Graham Gifford Graham Gifford
    I need to deflect a light beam from a fibre optic, through 90 degrees with a switchable system. The light is in the 190nm to 1100nm range. Is there a technology within the MEMS product range that could do this? Best Regards Graham Gifford
    on Dec 9, 2010
  • Forum Post: Source Code from Application Report DLPA009

    Judith Judith
    The Application Report DLPA009 shows code snippets from different sources, e.g. it mentions a file called "control.c". Does anyone know if these source files are available (for prototyping in a research project)?
    on Sep 14, 2010
  • Forum Post: Large MEMS pointing mirrors

    Stephanie Waite Stephanie Waite
    Hi, I was wondering what was the largest size available is for the MEMS pointing mirrors. I am looking for something with a 6 or 7 mm diameter. I some of the literature, the largest MEMS mirrors available is 5 mm diameter. Are specs available for a part that large? For the TALP1000B, is there any...
    on Sep 9, 2010
  • Forum Post: Alternative for TALP 1000B

    Jasna Azeez Jasna Azeez
    Sir, Can you suggest latest analog micro mirror other than TALP 1000B ? Please specify important applications of the same.
    on Jul 14, 2011
  • Forum Post: Re: TALP1000B magnets

    Arthur Turner Arthur Turner
    Hi Mike, We do have long term life test data on a different product that uses the same SmCo magnets. A total of 64 parts were actuated for >20,000Hrs at 60C with no significant increase in drive current (no change in magnitization). Regards, Arthur
    on Sep 23, 2011
  • Forum Post: Re: TALP1000B magnets

    Arthur Turner Arthur Turner
    Hi Mikhail, These devices are resoanant scanning mirrors. The error in the drive current measurement is +/- 5%. We saw no change to this level. Regards, Arthur
    on Sep 23, 2011
  • Forum Post: Re: Driver design for TALP 1000B

    Arthur Turner Arthur Turner
    Hi Jasna, Could you provide a basic application description (use the mirror in a pointing or scanning mode) and a basic discription of your PWM drive circuit. These will help us better answer your frequency question. Regards, Arthur
    on Sep 28, 2011
  • Forum Post: Re: TALP1000B hard stop

    Arthur Turner Arthur Turner
    Hi Mike, The TALP1000B does have mechanical rotation stops. These stops limit the maximum rotation angles to a value between 5 and 6 degrees. Regards, Arthur
    on Sep 29, 2011
  • Forum Post: Re: TALP1000B hard stop

    Arthur Turner Arthur Turner
    Hi Mike, The rotation stops are an integral part of the design. The TALP1000B has 8 magnets which (in conjuction with the 4 drive coils) provide the torgue required for rotation. Four magnets are easily visible on the reflective mirror side and 4 additional magnets are attached to the underside of...
    on Oct 3, 2011
  • Forum Post: Re: TALP1000B magnets

    Arthur Turner Arthur Turner
    Hi Mike, Sorry I just now noticed you post. Average deflection efficiencies are calculated on the currents measured at constant angle, in this case, +/-5 degrees mechanical. "Average" means that only the +/-5 degree currents are used, small non-linearities produce slightly different deflection...
    on Oct 4, 2011
  • Forum Post: Re: TALP1000B hard stop

    Arthur Turner Arthur Turner
    Hi Mike, TI recommends that the TALP1000B be operated within the data sheet operational angle specification which is +/-5 degrees mechanical for both axis. All qualification and reliability testing was restricted to this angle range. The mirror hinges can be damaged if a current corresponding to large...
    on Oct 6, 2011
  • Forum Post: Re: TALP1000B hard stop

    Arthur Turner Arthur Turner
    Hi Mike, The TALP1000B uses a push/pull type actuator. The coil winding and magnet polarities are arranged so that coil current pushes up on one magnet and pulls down on the other. There is no force on the rotation axis so there should be no sag. The previous statement is strictly true only for small...
    on Oct 6, 2011
  • Forum Post: Re: TALP1000B Replacement Recommendations?

    Arthur Turner Arthur Turner
    Hi Brad, TALP1000 m irror s were subjected to a tigh temperature life test as part of the qualification process. Devices were actuated the full 5 degrees mechanical at 60 Hz for 2000 Hrs at 85C. The sample size was 45 parts and both axes were driven using the same sinusoidal waveform rather than the...
    on Oct 18, 2011
  • Forum Post: Re: TALP 1000B

    Arthur Turner Arthur Turner
    Hi Ash, Applying 0.7V across pins 1 and 2 or across pins 11 and 12 should result in current flow in the circuit. Please verify that current is flowing (10mA for 0.7 V DC and 7.5mArms for 0.7 V AC). The current flow should result in mirror motion. If this is not the case then the divice may have been...
    on Nov 3, 2011
  • Forum Post: Re: Query Regarding Talp1000b

    Arthur Turner Arthur Turner
    Hi Vishal, The TALP1000B is an analog pointing mirror. It does not operate by moving in discrete angular steps. The voltage applied to the drive coils produces a current which results in mirror rotation. There is no minimum current increment for mirror rotation. If you are using a digital to analog...
    on Dec 5, 2011
  • Forum Post: RE: Query Regarding Talp1000b

    Arthur Turner Arthur Turner
    Greetings Vishal, The DAC7724 data sheet lists the maximum analog output current at 5mA. The TALP1000B requires up to 65mA of current to operate the mirror to full angle. The coil drive resistance of the TALP1000B is specified at 66 +/- 5 ohm. If 2.4V are placed across a 66 ohm load the resultant current...
    on Aug 2, 2012
  • Forum Post: RE: Query Regarding Talp1000b

    Arthur Turner Arthur Turner
    Greetings Vishal, Two possibilities are: The THS4222 DAC is capable of supplying up to 100mA. The OPA2830 is also a candidate. However, the specs in the OPA2830 datasheet show that it will work but it does not cover the entire range of the TALP1000B current drive (65mA). It can output 63mA...
    on Aug 2, 2012
  • Forum Post: RE: Optical Alignment using feedback [TALP100b]

    Arthur Turner Arthur Turner
    Hi Shailesh, The IPFx and IPFy position sensor parameters depend on the details of the LED emission and assembly tolerance. The parameters must be calibrated in angle during the system integration process. Typically the mirror is incorporated into the system and is then stepped through its operating...
    on Jan 16, 2013
  • Forum Post: RE: Re: SPIE Photonics West 2010 - visit the TI booth

    Pascal DLP Pascal DLP
    Rui, Welcome to the DLP & MEMS E2E forum. I notice that your question is posted in a thread that has not been active for a long time. The analog mirror products have been designated as EOL (End-of-Life), and are no longer recommended or available for new designs. This includes the TALP3001...
    on Mar 13, 2013
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use