I want to use the bare minimal control for manipulating the mirrors of a DMD device, the frame rate is 1 second per image so very slow, the question is can this be achieved with a programmable microcontroller such as ARM or PIC if the image is stored in the microcontroller then used to change the DMD image, during the 1 second the image is showing - the image in the microcontroller would then be refreshed to the next image.