Hi,
I am checking over the final specifications of the NIR scan before making a purchase and I just want to double check the spectral range.
If I take the following Raman Spectrum for methamphetamine, then it has a range approx. 400 through to 1800 cm-1. By my calculation this is a nanometer equivalent of 25000nm to 5555nm, in which case the spectral range of the NIR scan being 1350nm to 2450nm would be too limited.
I suspect an error in my conversion, so I would welcome any thoughts and comments.
Thanks,
Tom