Hi,
I am wondering if you have seen any documentation explaining the software structure for the NIR scan? What I mean is:
(1) What if I want to change the HTML pages so that I can customise the GUI?
(2) or better still if I want to write my own GUI what are the command structures which can be sent via USB/Eth?
(3) What if I want to change the firmware i.e. so I can create my own commands or automated some of the code - how do I compile this and is it all loaded from the SD card?
(4) I am interested to learn more about the optical path, so that I could change the configuration. Even better if simulation files were available?
(5) I think a high level document explaining the software hierarchy such that if say you wanted to change the HTML - you go into folder XYZ, if you want to use a command there is a list available showing accessibility from any of the ports (Web/Eth,USB), if you want to change the firmware then you will need such and such tools and programmer ...
I feel there are large sections of supporting material missing. The attraction for the DLP NIR scan for me is the advantage of the DMD, but I will want to create my own products from it, so I need this information and understanding. I feel that TI are almost treating this as a finished product rather than an open development tool which can be modified and replicated by the user/adopter.
Many Thanks,
Tom