• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » DLP & MEMS » All Tags » TALP1000B
Share
DLP & MEMS
  • Forums

Browse by Tags

DLP & MEMS

Welcome to the DLP & MEMS Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Sign In to Post
Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
TALP1000B
  • analog mirror
  • analog mirrors
  • Analog point mirror
  • axis
  • broken mirror
  • coil
  • current
  • DOA
  • MEMS
  • pointing mirror
Related Posts
  • Forum Post: Welcome to the MEMS Analog Mirrors Forum!

    rmeza rmeza
    Welcome to the MEMS Analog Mirror forum! For over a decade TI has developed and manufactured MEMS-based analog mirrors for optical applications. Now TI is offering its analog mirrors on ti.com. Feel free to use this forum to discuss applications and questions for the analog mirrors with the TI E2E Community...
    on Sep 18, 2009
  • Forum Post: TALP1000B samples available through TI eStore

    rmeza rmeza
    Based on feedback from its recent ti.com release, limited sample quantities of the TALP1000B dual-axis pointing mirror can now be purchased through the TI eStore. This eStore option allows purchase of 3 or 6 mirrors for evaluation. For quotes and availability of larger quantities of TALP1000B mirrors...
    on Dec 15, 2009
  • Forum Post: Analog mirror demos will be at SPIE Photonics West

    rmeza rmeza
    SPIE Photonics West will be January 26-28 in San Francisco. This year, you can check out demos using TI's analog mirror products (Booth #315) including a laser steering demo using the TALP1000B and a scanning mirror application for medical imaging. There will be several other demos featuring TI's...
    on Jan 4, 2010
  • Forum Post: Large MEMS pointing mirrors

    Stephanie Waite Stephanie Waite
    Hi, I was wondering what was the largest size available is for the MEMS pointing mirrors. I am looking for something with a 6 or 7 mm diameter. I some of the literature, the largest MEMS mirrors available is 5 mm diameter. Are specs available for a part that large? For the TALP1000B, is there any...
    on Sep 9, 2010
  • Forum Post: Source Code from Application Report DLPA009

    Judith Judith
    The Application Report DLPA009 shows code snippets from different sources, e.g. it mentions a file called "control.c". Does anyone know if these source files are available (for prototyping in a research project)?
    on Sep 14, 2010
  • Forum Post: TALP1000B devices arriving with broken mirrors

    Tim61732 Tim61732
    Hi, We ordered a sample TALP1000B device a few weeks back which arrived broken (mirror missing) & was replaced by the supplier Mouser UK. Last week I ordered a further two (again through Mouser UK) which arrived today both broken (one has mirror missing, the other detached). Given that two...
    on Dec 21, 2010
  • Forum Post: TALP1000B coil current

    sb57429 sb57429
    Hello, I just wanted to check if the coil current at maximum rotation applies for one coil or the whole axis as the circuit schematic looks like there are two coils in parallel per axis which would give me 130mA max. per axis. How much current can the mirror take per coil/axis max. (e.g. in case...
    on Jan 12, 2011
  • Forum Post: TALP1000B Replacement Recommendations?

    Bradford Chew Bradford Chew
    Since TI has announced that the TALP1000B is no longer recommended for new designs, does TI recommend a replacement for the TALP1000B? The TALP1000B works fine for my application. If TI is getting out of the analog MEMS business, has an alternate supplier been identified? Thanks! Brad
    on Jun 3, 2011
  • Forum Post: TALP1000B

    bibi mohanan bibi mohanan
    Hi, I am in search of the details about Analog point miror for a project. i want to know about TALP1000B and what does the "TALP" stands for?Is there any other analog point miror?What are the posible applications of Analog point mirror? Thank You
    on Jul 11, 2011
  • Forum Post: TALP 1000B driver and control loop

    Afsal M.K. Afsal M.K.
    Sir, I have planned to design scanning system using TALP 1000B based on Application report ( DLPA009). Can you send me updated driver and control loop design for the TALP 1000B. With regards, Afsal M.K.
    on Sep 16, 2011
  • Forum Post: Re: TALP1000B magnets

    Arthur Turner Arthur Turner
    Hi Mike, We do have long term life test data on a different product that uses the same SmCo magnets. A total of 64 parts were actuated for >20,000Hrs at 60C with no significant increase in drive current (no change in magnitization). Regards, Arthur
    on Sep 23, 2011
  • Forum Post: Re: TALP1000B magnets

    Arthur Turner Arthur Turner
    Hi Mikhail, These devices are resoanant scanning mirrors. The error in the drive current measurement is +/- 5%. We saw no change to this level. Regards, Arthur
    on Sep 23, 2011
  • Forum Post: Re: TALP 1000B driver and control loop

    Afsal M.K. Afsal M.K.
    Sir, Application report DLPA009 suggest a driver circuit as shown in Fig.2. I would like to get specification sheets of TLV2464,TPA721,MA3X198. When tried to search for these components multiple outputs are there. So please suggest me suitable one. If possible please include design for this circuit...
    on Sep 26, 2011
  • Forum Post: Source power required for TALP 1000B

    Afsal M.K. Afsal M.K.
    Sir, To scan an area of 4mmX4mm using TALP 1000B how much should be the power level of (Infrared Laser diode) source so that power per unit area is sufficient to reconstruct image of object . How can i estimate the same? PWM drive given for TALP 1000B suggest " The resonant frequency of the TALP1000B...
    on Sep 27, 2011
  • Forum Post: Re: Driver design for TALP 1000B

    Arthur Turner Arthur Turner
    Hi Jasna, Could you provide a basic application description (use the mirror in a pointing or scanning mode) and a basic discription of your PWM drive circuit. These will help us better answer your frequency question. Regards, Arthur
    on Sep 28, 2011
  • Forum Post: Re: TALP1000B hard stop

    Arthur Turner Arthur Turner
    Hi Mike, The TALP1000B does have mechanical rotation stops. These stops limit the maximum rotation angles to a value between 5 and 6 degrees. Regards, Arthur
    on Sep 29, 2011
  • Forum Post: Re: TALP 1000B

    Arthur Turner Arthur Turner
    Hi Ash, The TALP1000B mirror is coated with a Au reflecting surface that will reflect over 95% on the incident laser power (typically ~98% in the near IR). The TALP1000B has resonant frequencies (mirror and gimbals) near 120Hz. Scanning the mirror at 800Hz with drive powers below 700mW will result...
    on Oct 3, 2011
  • Forum Post: Re: TALP1000B hard stop

    Arthur Turner Arthur Turner
    Hi Mike, The rotation stops are an integral part of the design. The TALP1000B has 8 magnets which (in conjuction with the 4 drive coils) provide the torgue required for rotation. Four magnets are easily visible on the reflective mirror side and 4 additional magnets are attached to the underside of...
    on Oct 3, 2011
  • Forum Post: Re: TALP1000B magnets

    Arthur Turner Arthur Turner
    Hi Mike, Sorry I just now noticed you post. Average deflection efficiencies are calculated on the currents measured at constant angle, in this case, +/-5 degrees mechanical. "Average" means that only the +/-5 degree currents are used, small non-linearities produce slightly different deflection...
    on Oct 4, 2011
  • Forum Post: Re: TALP1000B hard stop

    Arthur Turner Arthur Turner
    Hi Mike, TI recommends that the TALP1000B be operated within the data sheet operational angle specification which is +/-5 degrees mechanical for both axis. All qualification and reliability testing was restricted to this angle range. The mirror hinges can be damaged if a current corresponding to large...
    on Oct 6, 2011
  • Forum Post: Re: TALP1000B hard stop

    Arthur Turner Arthur Turner
    Hi Mike, The TALP1000B uses a push/pull type actuator. The coil winding and magnet polarities are arranged so that coil current pushes up on one magnet and pulls down on the other. There is no force on the rotation axis so there should be no sag. The previous statement is strictly true only for small...
    on Oct 6, 2011
  • Forum Post: Re: TALP1000B Replacement Recommendations?

    Arthur Turner Arthur Turner
    Hi Brad, TALP1000 m irror s were subjected to a tigh temperature life test as part of the qualification process. Devices were actuated the full 5 degrees mechanical at 60 Hz for 2000 Hrs at 85C. The sample size was 45 parts and both axes were driven using the same sinusoidal waveform rather than the...
    on Oct 18, 2011
  • Forum Post: mirror driver

    Jasna Azeez Jasna Azeez
    Sir, Application report DLPA009 suggests MA 3X 198 for mirror driver. But MA 3X 198 is currently not available. MA 3S 133 is another switching diode,can i use this for mirror driver. If it is not possible please suggest an alternative. With regards, Jan
    on Oct 21, 2011
  • Forum Post: Re: TALP 1000B

    Jasna Azeez Jasna Azeez
    Hi, I have operated TALP 1000B with signal (amplitude 0.7V and frequency of 40Hz) based on application report DLPA007. But mirror is not working. Connector used to give signal to mirror through 1,2,11,and12. (without giving any support for MEMS mirror). Sir can you suggest a method to operate mirrors...
    on Nov 3, 2011
  • Forum Post: Re: TALP 1000B

    Arthur Turner Arthur Turner
    Hi Ash, Applying 0.7V across pins 1 and 2 or across pins 11 and 12 should result in current flow in the circuit. Please verify that current is flowing (10mA for 0.7 V DC and 7.5mArms for 0.7 V AC). The current flow should result in mirror motion. If this is not the case then the divice may have been...
    on Nov 3, 2011
12
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use