Is it possible to configure the DLP4710 EVM to display a side by side 3D video, and use the DLP-LINK glasses to watch the 3D video?
if yes, how to configure it?
thanks
jeffery
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, Nadine
Thank you for your reply, does TI provide the new firmware? I can upgrade the firmware with DLP LightCrafter Display v4.0 utility.
thanks
jeffery
Hello Jeffery,
I have sent you a message with the next steps. Please take a look.
Best regards,
Nadine
Nadine
it seems I can't access to the box. Could you share the image to me with other way, such as ftp or email?
the following error occurs when I try to view the folder which you have share to me.
sso.services.box.net/.../ACS.saml2
System Error
Sorry, an unexpected error condition has occurred. Please contact your system administrator for assistance and provide the following reference number to help locate additional information about this problem in the system log files.
Error Reference: iuglwu
Nadine
Finally, I have chance to test the 3D image, I have upgraded the image which you have sent to me successfully, but it still works in 2D mode, how can I set the EVM into 3D mode? (I think the left video should be overlay with right video without DLP-LINK glasses).
thanks
jeffery
Hello Jeffery,
You have to switch to look 3 in advanced mode of the GUI.
Best regards,
Nadine
Nadine
I followed your guide to set look 3 in advanced mode, and have tried 2 types of video format:
1. Blueray 3D DVD
the video is flicking with left and right video swapping.
2. 1080P side by side half 3D
I supposed the EVM should scale up the left side and right side then override those frames on the screen, but it does nothing, just display the half 3D video side by side.
do I need some special software to play the 3D video for EVM?
thanks
jeffery
Nadine,
Can you send me also the 3D firmware for the 4710evm devkit. I need the half hdmi frame rate synchronization for our compressive sensing application.
Thank you for your reply. My Email: fberier@evosens.fr
Regards
Frederic B.
Hello Frederic,
Thank you for your interest in our DLP technology.
Can you please let me know which DLP LightCrafter Display 4710 EVM you are using ? Are you using the Gen2 ?
Would you like to use 3D or are you only interested in the 120Hz frame rate.
Thanks,
Nadine
Hello Frederic,
Can you provide us your email that was used to create your TI.com account? This will provide us the ability to get you the firmware.
A few notes about using this:
The GPIO 9 (TRIG_OUT_B) signal requires the 3DR input signal from your host to function properly. Also R772 must be placed in order to see this signal out on the J48 connector, or else you can use TP79. You will have to move to LOOK #3 (the one that supports 3D) on the firmware we will provide you.
Look forward to hearing back from you!
Best,
~Danny W
Hi Danny,
I have seen on the schematics how to wire Trig_out_b. Thank you for the advice.
You can send me the firmware to fberier@evosens.fr
THank you very much
Frederic B
Hello Frederic,
Thanks for the prompt reply. You will be notified via email when the file is available for you to access. Please allow a day or two.
Best,
~Danny W