Hello,
In order to know about the characteristics of IT6801 HDMI receiver, I did replace the IT6801 chip mounted on an EVM board with new one.
What is first thing to do for the new IT6801?
After the replacement, the EVM is on the below status.
1. Without external HDMI input, the EVM is normally disaplaying an image(TI Logo) stored in EVM memory.
2. With external HDMI input (connected to PC)
- the EVM dosen't display any image.
- PC recognize the EVM as a monitor(ITE6801)
If there is no prolbem on the replaced IT6801, what shall I do to fix this problem.
Regards
Yun-Seok Cho