Other Parts Discussed in Thread: DLPC3439
Hi,
I am relatively new to DLP Lightcrafter 4710. For my 3D scanner application I need to trigger the projector through camera. How do I do that?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Ritaban,
Thanks for your interest in DLP products. Are you using the DLP4710_G2 EVM? If so please refer to a similar post which mentions how to use the triggers to sync a camera:
Also note that the DLP4710 is targeted at display applications and some processing is done to make images look better, therefore it's not pixel accurate. For a 3D scanner application I would recommend looking into our Advanced Light Control products which are pixel accurate and there are designs online for your application using these products, for example:
You can also refer to the E2E Advanced Light Control Forum for more support on these parts. Hope this helps.
Best,
Sepeedah
Ritaban,
Please let me take a step back and make a clarification on the 4710G2-EVM.
There is not a default trigger_in option available on the display chipsets including DLP4710. On the 4710G2-EVM, the available trigger to sync with a camera, is the trigger_out signals which are accessible as mentioned in the post that I referenced in my first response.
With that being said, the trigger_in pins noted in the 4710G2-EVM go to the MSP430 and may not be doing what you are looking to achieve. In order to understand their function, you will need to look into the MSP430 code and make necessary adjustments. The MSP430 is only capable of sending I2C commands to the DLPC3439 controller and drive proj_on high. Therefore, you need to see if you will be able to achieve what you are looking for with the I2C commands availabe and modify the MSP430 code if needed accordingly.
As a final note I would also like to mention that the display chipsets are not pixel accurate. Moreover for 3D scanner applications, many of our customers need to use binary patterns. Note that if you need binary patterns, they are not supported on this platform.
Best,
Sepeedah
Ritaban,
I think I misinterpreted your question. Please take a look at the EVM schematic found in this page:
If your purpose is to get access to those pins, they are accessible through J48 connector based on this schematic. However I will advise again that the DLP4710 chipset does not have a standard trigger in option. Therefore, you need to understand how the MSP430 is using those signals and if it will serve the purpose you are looking for.