I was wondering if it was possible to get a CAD model of the DLP 4710 Eval kit. I will be changing out the illumination source in the optics module and having these files will make the design of mounting brackets and the cooling system easier.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I was wondering if it was possible to get a CAD model of the DLP 4710 Eval kit. I will be changing out the illumination source in the optics module and having these files will make the design of mounting brackets and the cooling system easier.
Hello,
Thanks for using the DLP E2E forums! Have you taken a look at the design files published on the TI Design corisponding to the 4710EVM? They are located here:
Let me know if that helps!
~Danny W
Hi Danny,
Yes, I've already been through all these technical documents. I'm looking for 3D CAD files so that I can better understand the construction/geometry of the optics module, it's mounting to the other components, and specifically the heat-sink configuration on the DMD chip (i.e. does the DMD board have a pass-hole through it that allows direct contact between the heat sink and ceramic package). One of the technical PDFs (FLA7EVM Board Dimensions 071916.PDF found in the tidmc4.zip file) has isometric views from a 3D model, and this is what I'm looking to get. Is this possible? I know Nadine was sending out CAD files earlier, but maybe these are the ones that I've already reviewed and that you're pointing me to?
Thank you for your assistance.
Best Regards,
-David
Hello David,
We are working on getting a release that can be made public. We will update you when it is made available. Apologies for the inconvenience.
Best,
~Danny W