Other Parts Discussed in Thread: DLPC3439, DLPC4422
I'm curious if DLP4710 chipset can support 1920x1080 resolution at native 24hz frame rate without 3:2 pulldown. The technical spec says the maximum frame rate for the input signal is up to 60hz at 1080, but does not clearly mention that the output can be set to a lower rate.
In the mean time, I found a similar question on DLPC4422 saying that the chipset only recently got a firmware update for 24hz frame rate support with 2:2 pulldown, which might suppose the sibling DLP4710 didn't have 24hz support either.