Hi,
I am comparing different DMD chips and I have trouble finding the optical efficiencies in the Datasheet. Optical Efficiency is defined in the DLP3000 datasheet by the product of Window Transmission, Diffraction Efficiency, Mirror Surface Reflectivity and Fill Factor. It is equal to 68% for the DLP3000 which has a Diamond mirror layout.
Is it the same for TRP mirror layout like the DLP4710?
I have read here: that the new architecture is 30% more efficient. Is that the case?
Tchüss!
PS: I am also looking for the same information for the Manhattan architecture.