Hello
Just received my DLP 2000 EVM today....but from the quick start guide it is unclear if the BBB can power the DLP from his 5V DC input or if the DLP has to be powered separately...
The BBBW starts up normally, but no DLP startup screen is show, nor are any LEDs on...
Only if I unplug the DLP EVM and power it it shows the welcome screen...
Is the DLP EVM only compatible with the regular BBB but not the BBBW ?
thanks in advance
richard