I'm just curious if there's been any development since the inception of the DarkChip 4 DMD almost a decade ago to further reduce light scatter on the DMD level. For several years I've been excited hearing about all the uses that the VantaBlack carbon nano-tube material has brought to optical telescopes and other optical applications. Now I see that there is a spray on application that closely meets the original VantaBlack material for light absorption. This new Vantablack S-VIS nano-tube compound seems perfectly suited to be used as an extremely dark light absorption material that can be used behind the mirrors and even on the front facing housing to dramatically improve light scatter and improve on/off and ANSI contrast performance. Obviously the DMD chamber would also need to be coated in this material for the best contrast performance, but seeing how this part of the optical engine doesn't typically have a large surface area it could be coated with this material an a relatively cheap level.
I'm coming at this from a home theater projection perspective. I absolutely love a DLP image, but over the pasts 6 or 7 years the performance gains in contrast with reflective-LCD based technologies from JVC and Sony have increased to the point where DLP simply looks washed out by comparisons because the performance difference in contrast has widened immensely. There haven't been any meaningful increases in potential contrast performance on the DMD level since the DC4 DMD came out. I'm just hoping something like VantaBlack could potentially help.
Please feel free to comment if I'm mistaken, but couldn't something like VantaBlack help bring DLP closer to LCoS reflective-LCD panels in terms of on/off contrast performance given a manufacturer also used this material when designing the light engine?
If you're not familiar with VantaBlack, you can read about it here: