Hi,
I am interested in the DLPDLCR2010EVM development platform, mainly to get my hands on the DLP chip itself and the accompanying control board. In our envisioned setup the illumination would be provided by an external laser, so that we don't need the rest of the optics that come with this development platform.
My question is, whether it is (easily) possible to separate the optical module from the DLP and the control board. If this is the case, we would then like to mount the DLP on a home-made support. For this to work the DLP must be connected via a (reasonably long, maybe at least 5cm) cable with the control board - can you confirm this?
The laser wavelength we are using will be 780nm, so outside the given range of wavelengths for the DLP. Is it possible to order this development platform with the NIR version of the DLP? If not, could we order it separately and later exchange them?
Thank you very much in advance,
Kilian