Dear All,
Thank you for your support. Please let me ask you the DLP2010 chipset questions as below.
Best regards,
Rossinag
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear All,
Thank you for your support. Please let me ask you the DLP2010 chipset questions as below.
Best regards,
Rossinag
Hello Philippe
Thank you for your answers.
Please let me confirm my basic things.
1. There is not a formal sleep mode for your to toggle via I2C command, but the functional mode of the system can be toggled via the PROJ_ON pin. PROJ_ON is controlled by the front-end chip.
2. Please refer to section 1.1 of the software programmer's guide (www.ti.com/.../dlpu020a.pdf). As we can see in Figure 1, PROJ_ON is controlling the LED driver and controller at the same time. I also recommend you view the EVM reference design (www.ti.com/.../tida-00325) for more information on how to set up PROJ_ON.
Can the setting PROJ_ON low make the system to DMD parking and LED off after system power-on?
After above situation , can setting PROJ_ON high enable system wake-up?
3. Yes, the firmware does utilize the thermistor. In particular, it reads from the thermistor in order to maintain an internally-controlled temperature reading.
It seems the SENS2 of DLPA2000(5) connects to the temperature sensor(thermistor). Do you mean the DLPC3430(5) firmware utilize the SENS2's temperature sensor ? If so, is there a number of TI specified temperature sensor for DLPA2000(5)?
Best regards,
Rossinag
Rossinag,
"Can the setting PROJ_ON low make the system to DMD parking and LED off after system power-on?
After above situation , can setting PROJ_ON high enable system wake-up?"
This is correct.
"It seems the SENS2 of DLPA2000(5) connects to the temperature sensor(thermistor). Do you mean the DLPC3430(5) firmware utilize the SENS2's temperature sensor ? If so, is there a number of TI specified temperature sensor for DLPA2000(5)?"
I would like to direct you to the DLP2010EVM reference design, which can be located at http://www.ti.com/tool/tida-00325
If you check the implementation of the DLP board, you can see the implementation of the thermistor design which connects to SENS2 (link at http://www.ti.com/lit/pdf/tidrbl3)
If you have further questions, please let me know.
Regards,
Philippe Dollo
Dear Philippe,
Thank you for your support.
LcrDisplay2010EVM's thermistor seems to sense ambient temperature.
With regard to location of the thermistor , is there any place TI recommends?
Customer ask this question. Would you please provide advice?
Best regards,
Rossinag