Part Number: DLPDLCR2010EVM
Sorry if this sounds like a broken record, but is there firmware support to stream 120Hz from HDMI or something similar? If not, are there any tricks to get above 60Hz if one was willing to sacrifice resolution or color? Its kind of strange that the DLP and chipset claim to support 120Hz, but the eval module seems to only support 60Hz (unless this has changed with firmware). If not possible with the 2010, what is the most compact DLP that can do 120Hz+?
Thanks,
-Anthony