Part Number: DLPDLCR2010EVM
Hello,
I am planning on using a different optical engine than the one provided with the DLPDLCR2010EVM. The optical engine being used in based on the DLP2010 WVGA. From the wiring diagrams, inputs to the DLP2010 are labeled D_N/D_P for channels 1 to 4. However, on the EVM out connector (J1, AXT550124) there are HS_WDATA_N/HS_WDATA_P for channels A to H.
My question: Are these HS_WDATA channels driving the D_N/D_P channels on the DLP2010? Or am I missing something?
Thank you,
Dan