Part Number: DLPDLCR2010EVM
The lightcrafter EVMs seem to be split into two categories: 1) advanced light control and 2) display. My application is of advanced light control (optical microscopy). However, DLPDLCR2010EVM ($399) and DLPDLCR2000EVM ($99) are both cheaper and more current as compared to DLPLIGHTCRAFTER ($599). DLPDLCR2010EVM and DLPLIGHTCRAFTER also seem to have the same resolution. I would like to know if I can use DLPDLCR2010EVM or DLPDLCR2000EVM for my application. My requirements are as follows:
1) I need only binary pattern generation.
2) I am using an external light source, hence the optical engine/ led and optics should be detachable since I only want to use and control the DMD.
Please let me know which one will be better for my application.