I want to ask a question about the 8-bit refresh rate of the DLP3010. What does the 8-bit refresh rate mean? Does it mean the single color model? Or, does it mean the RGB trichromatic model?
How to calculate the RGB888 refresh rate of the DLP? Sometimes, I can get the maximum 8-bit refresh rate from the data sheets, but sometimes, I cannot find the data about the 8-bit refresh rate from the data sheet.So I want to known how to calculate the RGB888 refresh rate of the DLP. For example, what is the RGB888 color refresh rate of the DLP3010?
On the other hand, I want to known how to calculate the resolutions in the different refresh rate. If under the maximum refresh rate (120Hz), what can the resolution of the DLP3010 reach? And , the maximum refresh rate (120Hz ) means the 8-bit single color model, is it right? Please help me, and give me a detailed answer. Thank you very much.