Hello TI,
I have a DLP3010 EVM and want to trigger a TIS DMM 72BUC02-ML board level camera. Two other posts seem to indicate it is possible to get a camera trigger signal out of the 3010 EVM even though the module is in generally intended for display purposes. The first post linked below indicates the signal is available on TSTPT_4. Following TSTPT_4 from the DLP board (http://www.ti.com/lit/df/tidrcg8/tidrcg8.pdf) shows the signal should be available on TP2. Is this correct? I do not see signal on the scope. I would appreciate any information you are able to provide that would help to achieve this goal.
Thank you,
Zach
Similar forum posts: