Other Parts Discussed in Thread: DLP3010, DLPC300, DLPC3478
Hello,
is there a 1 bit binary pattern control (monochrome display as defined in the DLPC3000)?? if yes, which is the rates please.
Thanks and regards
Bastien
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Bastien,
The DLPC3433 is a display chipset, and as such is not optimized for sensing applications. At this time the DLPC3433 supports up to 120 Hz with 24-bit RGB input. Can you tell me more about the system you are trying to implement? I may be able to help you find the optimal chipset setup to use in this case.
I hope this helps.
Best Regards,
Philippe Dollo
Thanks for your reply
Actually we are working with the DLP3000 (associated to DLPC 3000 for display controller), this controller has RGB 24 bit input (as the DLPC3433) but propose a DMD output display frequency until 1440 hz max(1 bit monochrome external display feature )=> we control each mirror of the DMD at 1440 Hz.
Question is
*are this feature available on the DLPC3433 or is there other display controler which can provide this feature to drive the DLP3010? if not, i would like to know how are managed the mirror regarding the RGB input of the DLPC3433??
Thanks and regards,
Bastien