C5509A DSK Diagnostic Utility error

When I try and run the Diagnostic Utility for the 5509A DSK I get an error message when the utility opens.  The error message is: ERROR  Invalid working directory.  Any button I push (Start, Reset DSK, etc) causes the utility to crash.  When I look at properties for the Utility Desktop icon it shows that the working directory is \drivers folder under CCS install.  There doesn't seem to be anything related to the utility here.  Is there some type of installation error?

Additiona background.  I've got CCS3.3 Platinum installed, so per the QuickStart Guide I only installed the Target Content packages.  Could that have caused a problem?

Any help in resolving issue would be greatly appreciated.

Thanks.

 ---------------------------------------------------------------------------------------------------------

ACAT/DCAT Team

---------------------------------------------------------------------------------------------------------

Please click the Verify Answer button on this post if it answers your question.
---------------------------------------------------------------------------------------------------------