I hope this isn't too obvious a question but....
I've tried to locate 55xdsplib.exe on ti.com and failed. Can anyone tell me where to find it, please?
I'd like to be able to use the DSP functions, especially the FFT on the USB Stick development board, and dsplib seems to offer what I need.
Thanks,
Alex.
Ah ha! Found it at http://focus.ti.com/docs/toolsw/folders/print/sprc100.html
Thanks!
I was asking that myself this morning; thank you from Colorado
AliBali Ah ha! Found it at http://focus.ti.com/docs/toolsw/folders/print/sprc100.html Thanks!
I need the DSPlib too and it seems that the download is not there anymore. There is no link to download the lib. Or am I too blind!?
Could anybody tell me if I can download the DSPlib anywhere else? Pls help, thx :)
Okay guys I found it in the google cache
search for "cache:http://focus.ti.com/docs/toolsw/folders/print/sprc100.html"
Here the download-button is there!
But I want to to remember the admins that the download button is not there at the moment - so no one can load the DSPlib from your site :(
Hi,
Please use attached file.
Regards,
Hyun
---------------------------------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question.
Check out these great resources
http://processors.wiki.ti.com/index.php/Category:C5000---------------------------------------------------------------------------------------------------------
is "spru422j.pdf" still the reference? thank you, irvin
Yes it is.