Facing Problem in installing the software in Flash. The application only runs when the Debugger is used. It does not run in Standalone Mode
Hi C5000 Team,
The setup is C5515 based MDK with ECG frontend.
The issue is that the flashed code is not saved on power up. Is there a flash inside that can be used for standalone operation? Or are we missing some steps.
Can somebody please help?
Best Regards
Feroz
Feroz,
Please find the same question from the FAQ below.
http://processors.wiki.ti.com/index.php/C5515_EVM_FAQ
Regards,
Peter
Please click the Verify Answer button on this post if it answers your question.
It tried it but the application do no. The output of the programer application is:
Choose the device...1<filepath> - NOR Flash2<filepath> - NAND Flash3<filepath> - SPI4<filepath> - IIC EEPROM5<filepath> - MMC6<filepath> - SD2c:\Userdata\TEST\ECGSystem.binNAND Flash...Writing data to NAND...Writing Sector 0...Writing Sector 1 (MBR)...Flushing Data...Writing Boot Record...Flushing Data...Opening c:\Userdata\TEST\ECGSystem.bin...Input file openedWriting Boot-image to NAND...Programming... [TotalSize=256 (0x100)]Programming... [TotalSize=512 (0x200)]Programming... [TotalSize=768 (0x300)]Programming... [TotalSize=1024 (0x400)]Programming... [TotalSize=1280 (0x500)]Programming... [TotalSize=1536 (0x600)]Programming... [TotalSize=1792 (0x700)]Programming... [TotalSize=2048 (0x800)]Programming... [TotalSize=2304 (0x900)]Programming... [TotalSize=2560 (0xA00)]Programming... [TotalSize=2816 (0xB00)]Programming... [TotalSize=3072 (0xC00)]Programming... [TotalSize=3328 (0xD00)]Programming... [TotalSize=3584 (0xE00)]Programming... [TotalSize=3840 (0xF00)]Programming... [TotalSize=4096 (0x1000)]Programming... [TotalSize=4352 (0x1100)]Programming... [TotalSize=4608 (0x1200)]Programming... [TotalSize=4864 (0x1300)]Programming... [TotalSize=5120 (0x1400)]Programming... [TotalSize=5376 (0x1500)]Programming... [TotalSize=5632 (0x1600)]Programming... [TotalSize=5888 (0x1700)]Programming... [TotalSize=6144 (0x1800)]Programming... [TotalSize=6400 (0x1900)]Programming... [TotalSize=6656 (0x1A00)]Programming... [TotalSize=6912 (0x1B00)]Programming... [TotalSize=7168 (0x1C00)]Programming... [TotalSize=7424 (0x1D00)]Programming... [TotalSize=7680 (0x1E00)]Programming... [TotalSize=7936 (0x1F00)]Programming... [TotalSize=8192 (0x2000)]Programming... [TotalSize=8448 (0x2100)]Programming... [TotalSize=8704 (0x2200)]Programming... [TotalSize=8960 (0x2300)]Programming... [TotalSize=9216 (0x2400)]Programming... [TotalSize=9472 (0x2500)]Programming... [TotalSize=9728 (0x2600)]Programming... [TotalSize=9984 (0x2700)]Programming... [TotalSize=10240 (0x2800)]Programming... [TotalSize=10496 (0x2900)]Programming... [TotalSize=10752 (0x2A00)]Programming... [TotalSize=11008 (0x2B00)]Programming... [TotalSize=11264 (0x2C00)]Programming... [TotalSize=11520 (0x2D00)]Programming... [TotalSize=11776 (0x2E00)]Programming... [TotalSize=12032 (0x2F00)]Programming... [TotalSize=12288 (0x3000)]Programming... [TotalSize=12544 (0x3100)]Programming... [TotalSize=12800 (0x3200)]Programming... [TotalSize=13056 (0x3300)]Programming... [TotalSize=13312 (0x3400)]Programming... [TotalSize=13568 (0x3500)]Programming... [TotalSize=13824 (0x3600)]Programming... [TotalSize=14080 (0x3700)]Programming... [TotalSize=14336 (0x3800)]Programming... [TotalSize=14592 (0x3900)]Programming... [TotalSize=14848 (0x3A00)]Programming... [TotalSize=15104 (0x3B00)]Programming... [TotalSize=15360 (0x3C00)]Programming... [TotalSize=15616 (0x3D00)]Programming... [TotalSize=15872 (0x3E00)]Programming... [TotalSize=16128 (0x3F00)]Programming... [TotalSize=16384 (0x4000)]Programming... [TotalSize=16640 (0x4100)]Programming... [TotalSize=16896 (0x4200)]Programming... [TotalSize=17152 (0x4300)]Programming... [TotalSize=17408 (0x4400)]Programming... [TotalSize=17664 (0x4500)]Programming... [TotalSize=17920 (0x4600)]Programming... [TotalSize=18176 (0x4700)]Programming... [TotalSize=18432 (0x4800)]Programming... [TotalSize=18688 (0x4900)]Programming... [TotalSize=18944 (0x4A00)]Programming... [TotalSize=19200 (0x4B00)]Programming... [TotalSize=19456 (0x4C00)]Programming... [TotalSize=19712 (0x4D00)]Programming... [TotalSize=19968 (0x4E00)]Programming... [TotalSize=20224 (0x4F00)]Programming... [TotalSize=20480 (0x5000)]Programming... [TotalSize=20736 (0x5100)]Programming... [TotalSize=20992 (0x5200)]Programming... [TotalSize=21248 (0x5300)]Programming... [TotalSize=21504 (0x5400)]Programming... [TotalSize=21760 (0x5500)]Programming... [TotalSize=22016 (0x5600)]Programming... [TotalSize=22272 (0x5700)]Programming... [TotalSize=22528 (0x5800)]Programming... [TotalSize=22784 (0x5900)]Programming... [TotalSize=23040 (0x5A00)]Programming... [TotalSize=23296 (0x5B00)]Programming... [TotalSize=23552 (0x5C00)]Programming... [TotalSize=23808 (0x5D00)]Programming... [TotalSize=24064 (0x5E00)]Programming... [TotalSize=24320 (0x5F00)]Programming... [TotalSize=24576 (0x6000)]Programming... [TotalSize=24832 (0x6100)]Programming... [TotalSize=25088 (0x6200)]Programming... [TotalSize=25344 (0x6300)]Programming... [TotalSize=25600 (0x6400)]Programming... [TotalSize=25856 (0x6500)]Programming... [TotalSize=26112 (0x6600)]Programming... [TotalSize=26368 (0x6700)]Programming... [TotalSize=26624 (0x6800)]Programming... [TotalSize=26880 (0x6900)]Programming... [TotalSize=27136 (0x6A00)]Programming... [TotalSize=27392 (0x6B00)]Programming... [TotalSize=27648 (0x6C00)]Programming... [TotalSize=27904 (0x6D00)]Programming... [TotalSize=28160 (0x6E00)]Programming... [TotalSize=28416 (0x6F00)]Programming... [TotalSize=28672 (0x7000)]Programming... [TotalSize=28928 (0x7100)]Programming... [TotalSize=29184 (0x7200)]Programming... [TotalSize=29440 (0x7300)]Programming... [TotalSize=29696 (0x7400)]Programming... [TotalSize=29952 (0x7500)]Programming... [TotalSize=30208 (0x7600)]Programming... [TotalSize=30464 (0x7700)]Programming... [TotalSize=30720 (0x7800)]Programming... [TotalSize=30976 (0x7900)]Programming... [TotalSize=31232 (0x7A00)]Programming... [TotalSize=31488 (0x7B00)]Programming... [TotalSize=31744 (0x7C00)]Programming... [TotalSize=32000 (0x7D00)]Programming... [TotalSize=32256 (0x7E00)]Programming... [TotalSize=32512 (0x7F00)]Programming... [TotalSize=32768 (0x8000)]Programming... [TotalSize=33024 (0x8100)]Programming... [TotalSize=33280 (0x8200)]Programming... [TotalSize=33536 (0x8300)]Programming... [TotalSize=33660 (0x837C)]Flushing Data...Programming Complete
C5515 eZDSP...Input <filepath>c:\Userdata\TEST\ECGSystem.binNOR Flash...Erasing chip (NOR)...Opening c:\Userdata\TEST\ECGSystem.bin...Input file openedWRITE ERROR! at 0x00000000Wrote 0x5e80 Read 0x00b2
Hello Mr. Aseem,
is this issue resolved. If yes, please verify close this item.
Else, please share the snapshot - upload it here.
No the problem has not been solved.