Hi!
I am trying to achieve the following:
1. I have a PC program that sends/receives speech samples to/from DAC/ADC.
Speech samples are taken at 8KHz at 16 bits / sample. I understand eZDSP USB stick
has built-in DAC/ADC. However, I have to use DAC/ADC which is already in use in the PC.
2. I would like to send the speech samples acquired in 1 above from PC to DSP
via USB interface of eZDSP C5515.
3. DSP will process the speech samples.
4. DSP will send the processed speech samples back to PC via the USB interface of eZDSP USB stick.
Here comes my questions!
1. To achieve these, do I need USB driver to work with the eZDSP USB stick? Does the eZDSP USB stick
come with the proper driver for win2000 server? If not, how can I get the proper driver?
2. Can you show me an PC example code in C how to send/receive speech samples to/from DSP
utilizing the USB driver?
3. Can you show me an DSP example code in C for eZDSP USB stick to receive/send speech samples from/to
PC utilizing the USB driver?
Thanks.
BR
HG KIM
PS: If eZDSP 5515 is hard to achieve my goal, then please advice me other DSP board or DSP card that is more proper.