Hi
I am a DSP-noob experimenting with a C5505 eZdsp. For the moment I am trying to do some filtering with help of dsplib (http://processors.wiki.ti.com/index.php/DSPLIB), especially with iircas5. I can't get it to work though.
Firstly, what is the format of the coefficients to use when calling?
C55x DSP Library Programmer’s Reference Manual says: h = a11 b11 a21 b21 b01
The attached examples says: h = a1 a2 b2 b0 b1
Below is a delcaration of a filter with coefficients according to the second model (allthough Im not sure if it's good coefficients in the first place)
/* TEST FILTER */ushort test_NX = 1; // Number of elements of input and output vectorsushort test_NBIQ = 1; // Number of biquadsDATA test_h[5] = {13, 7, 15499, 16384, -31857}; // Filter coefficients 300 Hz LPDATA test_dbuffer[4]; //delay line d format:DATA *test_dp = test_dbuffer;
In main, the function is called by: iircas5(&right_input, test2_h, &left_output, test2_dp, test2_NBIQ, test2_NX);
Secondly, I have a problem finding coefficients for low cutoffs. If I scale them so that the largest (a1) fits the 16-bit int used by DSP-lib, the lowest values (b0, b2) are lower than 1.
What I want to have is a 30 Hz lowpass filter to extract the envelope of an audio signal in realtime. Is IIR what I should be looking for at all?