CCS Version: 4.2.5.00005
CSL Version 2.50.000
Trying to load the UART example project from:
C:\Program Files\C55 Low Power Chip Support Library v2.50.00\c55xx_csl\ccs_v4.0_examples\uart
into my CCS workspace. I Get the following error: Other post relating to this generic issue talk about using newer versions of the tools, but according to the doc, all the csl examples were tested using ccs v4.1 and I am using a newer version of ccs, so i'd expect backwards compatibility. Any ideas?
----- Please click the Verify Answer button on this post if it answers your question --------
I personally is using 4.2.4.00033. According to this from CCS wiki, 4.2.5 is "Patch only". Does it mean 4.2.4 is needed?
http://processors.wiki.ti.com/index.php/Download_CCS
-------------------------------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question
--------------------------------------------------------------------------------------------------------
I've isolated the issue. It is with my existing install of CCS. The C5500 device support was not installed when i first put CCS on my machine. I've started a new thread to address this issue on the CCS site:
http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/p/186723/672197.aspx#672197