Hi,
I have TMDX5535EZDSP kit and I have been working on the sine wave examples. If I am not mistaken, C5535 uses the sine wave constants and makes the calculations according to fixed-point feature. I can only create two outputs since the kit has two headphone outputs (left and right) via AIC3204 codec.
I would like to create 8 different sine wave outputs (10kHz-30kHz range) from the kit. Is that possible with C5535? If so, how can I do it? If not, why and what should I use instead?
I was thinking of using 4xAIC3204 in parallel to generate the sine waves?
Thanks for advance