Hello,
I want to use FAT on SD card with my board based on DSP C5535.
I can see that there is an example with ATAFS in CSL v3.01,
however it seem that the project is a RTSC project with BIOS since there is a Bios config file and task running.
This is needed by the ATAFS lib which is compiled with BIOS.
In my project is a standard CCS project. I don't need to use BIOS an multitasking but I want to use ATAFS.
Is there any solution to compile the code of ATAFS without the use of BIOS RTOS?
If not is there any other FAT file system which can work with the 16 bit only architecture of C55 familly?
Regards,
Max