I want to get a kit called DDK, but i cant find in the TI web. i hope someone can tell me the palce, or gvie me one. and i want to get a complete one. thank you very much ......
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I want to get a kit called DDK, but i cant find in the TI web. i hope someone can tell me the palce, or gvie me one. and i want to get a complete one. thank you very much ......
Hi
Please refer to the following post
http://e2e.ti.com/support/embedded/tirtos/f/355/t/195217.aspx
This is an old and depricated software product , so we do not recommend you start with this.
Please consider evaluating newer c55x devices instead of C5509A, if you are starting a new development.
Regards
Mukul
I also want to know that wither i can used DDK 1.20 or 1.10 with CCS3.3, and the new version DDK is ? thank you very much.
There is no newer version of DDK.
On which version works with which CCS release, if this is not clear from the release notes etc, please try to post a query on the TI RTOS forum to see if someone can provide additional pointers
http://e2e.ti.com/support/embedded/tirtos/default.aspx
Again, this is an older software package, so you are likely going to find very little information on this.
Regards
Mukul