Dear:
I have design a 5509 system and fond a problem, which is: when the rest of dsp is powered down, the rtc power will be used up very soon, about one weed.
Because of that I measured the current and I found the the current can goes up to 15uA, sometimes can goes upto 1mA, is that ok?