Dear All,
According to the web page "USB made simple Part - 3 Data Flow" :
http://www.usbmadesimple.co.uk/ums_3.htm
:
It is also possible for a device with its remote wakeup feature set, to initiate a resume itself. It must have been in the idle state for at least 5ms, and must apply the wakeup K condition for between 1 and 15 ms. The host takes over the driving of the resume signal within 1 ms.
:
USB Device may issue 1ms~15ms K condition to Host as a signal for remote wakeup. The RWUP (Bit5) of C5509A's register USB Control Register (USBCTL) is for this purpose. However, it seems that there is not other register to control the duration of this signal.
As I encountered an USB compatibility issue, which may be solved by adjusting that duration, I'm wondering if I can adjust the duration of the remote wakeup signal issued by C5509A?
Regards,
Oliver