All,
I am using the C5505 with CSL ver.3.04.00 and DSP-BIOS version 5.42.01.09
I use SPI to initialize an attached FPGA, using 12-bit SPI mode, and it seems to work fine with CSL ver. 2.5. However, it does not work with CSL ver.3.04, it seems to me that the code (function SPI_write(...) supports only 8-bit and 16-bit modes.
Is my 12-bit mode work supported ?
Arie