Hello.
Could you explain me how to connect TMS320LC549 and parallel EEPROM (16bit) (AM29, for instance) to load programm during boot?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello.
Could you explain me how to connect TMS320LC549 and parallel EEPROM (16bit) (AM29, for instance) to load programm during boot?
Hi,
Team is working on it and will provide an update shortly.
Thanks & regards,
Sivaraj K
May I ask the reason for this inquiry? LC549 is not recommended for new design. Informations about this device is very limited.
Regards.
I'm working in Testing company, so this DSP is used by our customer. I don't know why they use it :) But I have to test this DSP for them
Ok. I would assume you are testing the DSP by itself then. You willl connect the EMIF interface. The best example I can think of is the DSP Development Board application note, Refer to Figure 21 and 22 for connecting the 16 bits data bus.
http://www.ti.com/general/docs/lit/getliterature.tsp?baseLiteratureNumber=spra465&fileType=pdf
Secondly, parallel boot mode is the second mode of the bootloader after HPI. INT2 idle indicates non-HPI boot. This device supports a vast varieties to boot from external data memory space. Details of how the bootloader works is documented in the Bootloader application report.
http://www.ti.com/general/docs/lit/getliterature.tsp?baseLiteratureNumber=spru288&fileType=pdf
Hope this help.