Hello.
I do not have enuf room for all my code in the internal RAM of the C5515.
Could I run code directly from the extenal NOR of the EVM?
Thank you.
David,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello.
I do not have enuf room for all my code in the internal RAM of the C5515.
Could I run code directly from the extenal NOR of the EVM?
Thank you.
David,
Hi,
Team is looking in to this and will address your query shortly.
Thanks & regards,
Sivaraj K
Hi,
The below e2e post provides details on How to run the code from external memories.
http://e2e.ti.com/support/dsp/c5000/f/109/t/195227.aspx
http://e2e.ti.com/support/dsp/c5000/f/109/t/345423.aspx
Hope this helps.
Regards
Vasanth
1) Can I read about this in a formal ti document?
2) How do I load the code in to the NOR Flash for debugging?
3) I can tell the linker to put code in the NOR code space with the pragma directive. but
I want to know the limitations. - will this code run slower?
There isn't a formal application note for this. Debugger applies to internal memory becuase it is the executed memory space. The memory space for NOR is limited by the external-CS space specified in Memory Map Summary figure.
Regards.
What do you mean by "Debugger applies to internal memory"?
Can I debug code that runs on the EVB NOR - or not?
If YES - What are the limitations for debugging on the EVB NOR Flash?
If NO - what is the problem?