I have installed the CCS6 and working with it using othe JTAG adapter.
I bought a new Blackhawk USB560 V2.
How do I install the drivers to use it?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have installed the CCS6 and working with it using othe JTAG adapter.
I bought a new Blackhawk USB560 V2.
How do I install the drivers to use it?
What problem do you have? They ususally shipped with a CD. Have you checked with Blackhawk's site?
Regards.
I am running on Win7 x64 Lenovo laptop
Blackhawk's CD says program not compatible.
Blackhawk's site links to ti's ccs
I have CCS6 installed and updated but
When I connect the device windows says there is no compatible driver.
Have been using BH-USB-560M/Win7/CCS5.5.0 without any problems for ~1yr without problem. Have not used CCS6 nor Lenovo. Maybe swicth to CCS5.5 for C55 since all C55 were developed on CCS5.5.
Regards.
I need to use other MCU that is not supported on the CCS5 vertion.
Can you please test if you can use the CCS6?
found the problem.
I had both CCS6 and CCS6.01 mixed on my machine.
I am cleaning everything and starting over.
If I will have more problems I will post them.