Hello,
I've a 5515evm running well with the ADS1298. Next I used the SmartRF with cc2540/41 to create a bi-directional serial connection. This works fine as well. However it seems to me that, checking the schematics (5515EVM and CC2540EM), the Rx (P0.2) and Tx(P0.3) are in conflict with the Rx/Tx signals on the 5515EVM module! Can someone confirm this? Before I start patching!
kind regards,
Laurent