When I declare #include<usbstk5515.h> , CCS 6 can't debug. It said that CCS 6 can't open usbstk5515.h file in include directory. Can anyone help me ? What I have to do ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
When I declare #include<usbstk5515.h> , CCS 6 can't debug. It said that CCS 6 can't open usbstk5515.h file in include directory. Can anyone help me ? What I have to do ?
Hi,
Team will work on this and will provide an update as soon as possible.
Thanks & regards,
Sivaraj K
Alfonsus,
The board-specific headers do not come with CCS. Please take a look at the Spectrum Diginal support page for 5515 eZdsp USB Stick:
http://support.spectrumdigital.com/boards/usbstk5515/reva/
Download the Test Code for CCS 4.1. This can be imported to CCS v5 and v6. This will contain examples, as well as the Board Support Library with the usbstk5515.h that you are seeking.
Hope this help.
-Jon
I would recommend to install the C55XCSL-LOWPOWER software and follow the steps in Chapter 3 " For Running the Projects on C5504/05/14/15 DSP" for C5515_EZDSP:
http://www.ti.com/tool/sprc133
Regards.